Postings tagged with: radar


Herman Coello| Feb 04, 2016

grain

Don’t get lost in the maize at GEAPS

If you have been tracking GEAPS’ progress over the years, GEAPS 2016 is said to be the biggest and largest in its history. I recently read an article stating that because it is such a large event, it may be intimidating to navigate through it. True, this is an event where people from all over the globe converge to be educated, find solutions or simply meet face-to-face with other folks in the industry. Visiting everyone you have in mind may not even be possible due to its sheer size! I, personal ...

Herman Coello| Sep 03, 2015

1 comment

HC Flour Blog 08102015

How do you level your issues with flour?

It is pretty amazing the many types of goodies that you can create with flour. These creations require various types of flour and some of these flours, because of their composition, are tougher than others to accurately measure their levels in a silo. To the flour mill producer, the characteristics of each type of flour allows for the right recipe blend. In the milling process, production goes hand-in-hand with inventory. It happens that the various characteristics that flour exhibits from crop- ...

Jonas Norinder| May 14, 2015

chemical blog - case study

How do you increase batch process safety in a silo?

Over the past few months, my colleague, Michael Sherenian, and I have covered several aspects related to tank overfill protection and how to design a system with focus on safety. Although today’s topic is not related to tank measurement or overfill protection, it is still associated with plant safety and reducing workplace hazards. When you think of chemical plant hazards, what usually comes to mind? Chemical exposures, poisoning, and fires or explosions due to volatile changes in the chemical m ...

Herman Coello| Jan 21, 2015

Grain Level Jan2015 Blog

How can you simplify your grain level measurement?

Here is the situation: a grain handling company in Minnesota needed level measurement for a cluster of eight grain silos. This seemed like a usual, run-of-the-mill request. However, the cluster consisted of six 120 foot tall concrete silos that were arranged in such a way that they formed additional storage, which resulted in two interstice or star-bin silos. Narrow tall silos present problems of their own, but the more complex geometry of interstice or star-bin silos is truly a challenge for mo ...

Herman Coello| Dec 04, 2014

2014 National Sales Meeting - LR560 Challenge

Got a minute?

That is pretty much what we have these days to do certain things. Configuring process instruments generally takes a quick skimming of the manual before the actual device setup is even attempted.Over two years ago when we released SITRANS LR560, the first 78GHz radar level transmitter, we knew that it could be set up in minutes using the quick wizard and graphical user interface.  We love to see people who never touch an instrument be amazed when they set the LR560 in just a few minutes. In a rec ...

Herman Coello| Oct 15, 2014

radar-level-LR250-group-blog

Product Spotlight: LR250 Hygienic Encapsulated Antenna

Siemens is introducing the latest addition to the SITRANS LR250 family, the LR250 Hygienic Encapsulated Antenna (HEA). The LR250 HEA offers  a fully encapsulated antenna with no air gaps behind the lens, thus preventing unwanted moisture build-up. This instrument has the flexibility to be used in sanitary processes and harsh environments, which is accomplished with its leading-class hygienic process connections. The SITRANS LR250 HEA uses compliant materials according to FDA and USP Class VI, an ...

Michael Sherenian| Jul 08, 2014

Chemical-Blog-Sherenian

Stop risking it all and learn how you can prevent your tank from overfilling

While storage tank overfills are certainly not new to the chemical industry, overspills and leaks are happening on a frequent basis and don’t seem to be slowing down anytime soon. Already, 3,007 incidents have been reported to the EPA this year alone. That many overfills translates into a lot of damage that’s occurring to your employees’ safety, the environment, and your budget …and it’s only mid-year!So, in the age of information and new technology, why are overfills still happening?There are m ...

Herman Coello| Jun 12, 2014

cement part2 blog image1

Do you have a challenging level application in cement?

Hello again! On my previous blog dealing with level instruments in the cement process, I focused on level technologies that are well-suited for the dusty environment found in the cement industry. Moving forward with our discussion, you’ve probably noticed that microwave technology or solid level radar transmitters (SLR) stand out as the preferred choice in many of the level applications in the production process. High frequency microwave radar transmitters are ideal for dusty environments. The t ...

Herman Coello| May 07, 2014

cement v4

Strong growth within the cement industry is bound to require solid level measurement

Although last year’s forecast on cement was not as high as expected, there was still growth within the industry due to commercial and residential building. This year is projected to be a better year and the trend is said to continue at least until 2018. With the industry picking up speed, do you have a concrete idea of what level transmitters you will need to better manage your process?The industry has obviously changed in the turmoil. As personnel moved, some expertise moved as well.  It’s with ...

Herman Coello| Feb 28, 2014

Horn Antenna

How do you choose the right level instrument for chemically aggressive environments?

Okay, so you need to know the level on one of your tanks and you are wondering which level transmitter instrument will meet your needs.  The tank calls for a bit more attention because the material in it is chemically aggressive.  From past experiences, you know that similar tanks do not work well with instrumentation tools or costly exotic construction materials, like Hastelloy alloys.Even if choosing the right technology may not be an issue for you, you may still be interested in a level appli ...


 previous
close