Postings tagged with: process news


Carolin Paravan| Mar 17, 2016

StocExpo 2016

Digitalization the talk of the town at StocExpo 2016

The StocExpo 2016 in Antwerp will come to an end in only a few hours from now. However, following three days of numerous interesting discussions with clients, manufacturers and system partners about latest tank storage trends and innovations, there is widespread agreement that the gathering was once again a highly informative and well worth the visit.Despite the stressful networking schedule, we are returning home highly pleased with the sales leads we were able to generate as well as the opinio ...

Carolin Paravan| Mar 16, 2016

Tank Farming

Finely tuned instrumentation enabling sound returns

Inventory monitoring, overspill protection and loss control, emissions monitoring, leak detection and localization and, of course, product metering – these are tasks that all bulk storage facilities deal with everyday. One thing they all have in common is the need for reliable and accurate information on stock inventories and movements. Newly developed tank level monitoring instrumentation from Siemens, for example, incorporates advanced software algorithms for highly accurate continuous tank le ...

Adam Wesoly| Jun 29, 2015

From integrated engineering to integrated operation - the expert public could learn more about data integration with Comos and Simatic PCS 7 at ACHEMA 2015

ACHEMA 2015: The expert public reviews digitalization

Discover the potential of digitalization – this was not just the motto of our ACHEMA 2015 show. On our booth, we had a liquid circulation model on display that demonstrated how data integration between engineering and operation works and how the digital and physical plant interacts. What did the experts say about this exhibit? Here’s our report. Maik Friedrich, one of our marketing managers at ACHEMA, provided us with a short description of the exhibit:  “What we can see here is a relatively si ...

Adam Wesoly| Jun 29, 2015

Vom integrierten Engineering zum integrierten Betrieb - Fachbesucher konnten sich auf der ACHEMA 2015 über die Datenintegration zwischen Comos und Simatic PCS 7 informieren

ACHEMA 2015: Die Digitalisierung stellt sich den Fragen des Fachpublikums

Entdecken Sie das Potenzial der Digitalisierung – das war nicht nur Teil unseres Mottos für die ACHEMA 2015, sondern auch das konkrete Thema eines unserer Exponate. Am Modell eines Flüssigkeitskreislaufs präsentierten wir die Datenintegration zwischen Engineering und Betrieb und zeigten, wie reale und digitale Anlage interagieren. Was sagte das Fachpublikum dazu? Hier unser Bericht. „Was wir hier sehen, ist ein einfaches Modell eines Flüssigkeitskreislaufs. Trotzdem sind praktisch alle Komponen ...

Adam Wesoly| Jun 25, 2015

content

ACHEMA 2015: The seven trials of an I/O module

Sometimes, our engineers like a good challenge. Recently, one of our IO modules was the subject of an especially demanding study: The Simatic ET 200AL I/O for installation without control cabinet was put to the test. Seven trials were scheduled to find out whether the tiny module really complies with the standards for IP65/67 degree of protection, one including a burner. The result: Simatic ET 200AL may be small, but it is one tough cookie. Every event has its special moments. You stroll around ...

Adam Wesoly| Jun 25, 2015

content

ACHEMA 2015: „Siebenkampf“ für eine Baugruppe

Manchmal können unsere Ingenieure echt ganz schön herausfordernd sein. Für unsere Simatic ET 200AL Baugruppe, mit der wir Signale auch ohne Schaltschrank im Prozess an die Automatisierung anbinden können, hatten sie sich eine besondere Prüfung ausgedacht. Sozusagen eine Art „Siebenkampf“ für IP65/67 Baugruppen – unter anderem kam dabei eine Gasflamme zum Einsatz. Das Ergebnis? Unsere Simatic ET 200 AL ist ein echter Modellathlet. Es gibt sie manchmal, diese besonderen Momente auf Messen. Beim G ...

Adam Wesoly| Jun 18, 2015

1 comment

The better choice of coupling for the process industry -  our N-BIPEX

ACHEMA 2015: Premiere for the new star among our couplings

ACHEMA is the perfect occasion to introduce our new products to a big crowd. This year, we had a true world premiere: the new N-BIPEX challenges the other couplings on the market by claiming to be the “better choice of coupling for the process industry”. Does it have what it takes? Here’s our report. Our latest addition to the Flender product range makes quite a few claims – higher torque, improved safety, lower costs. It says it can even extend the service life of the entire drive train. Now, ...

Adam Wesoly| Jun 18, 2015

Die bessere Kupplung für die Prozessindustrie – unsere N-BIPEX

Achema 2015: Premiere für den neuen Star bei unseren Kupplungen

Die Achema ist wie immer auch der ideale Ort, um unseren Besuchern neue Produkte zu präsentieren. Dieses Jahr gab es sogar eine echte Weltpremiere: die neue N-BIPEX Kupplung. Sie tritt an, um „die bessere Kupplung für die Prozessindustrie“ zu sein – ganz schön ehrgeizig, die Kleine. Das jüngste Mitglied in unserer Flender Getriebefamilie verspricht so einiges: Drehmoment steigern, Sicherheit erhöhen, Kosten senken. Und auch noch die Lebensdauer des gesamten Antriebsstranges verlängern. Wie das ...

Adam Wesoly| Jun 18, 2015

content

ACHEMA 2015: An integrated power supply in the process industry? It’s a safe bet with Totally Integrated Power

We first notice how important a functioning power supply is when it’s no longer there – for example during a power failure. In production environments, this is not only a nuisance but also a huge cost risk.A stable power supply is particularly critical in the process industry – in other words, an uninterrupted, secure supply of power must be ensured at all times. This is not only applicable to failures but also to fluctuations in the power quality – otherwise, it’s not only the systems that stop ...

Adam Wesoly| Jun 17, 2015

content

Achema 2015: Durchgängige Energieversorgung in der Prozessindustrie – sicher mit Totally Integrated Power

Wie wichtig eine funktionierende Stromversorgung ist, stellt man dann fest, wenn sie nicht gewährleistet ist – zum Beispiel bei einem Stromausfall. Vor allem in der Produktion ist dies nicht nur unangenehm, sondern kann schnell richtig teuer werden.Die Prozessindustrie ist in punkto Energie besonders versorgungskritisch – d. h. es muss eine kontinuierliche, sichere Versorgung gewährleistet sein. Dies gilt nicht nur für Stromausfälle, sondern auch für Schwankungen in der Stromqualität, ansonsten ...


 previous
close