Tools


Siemens Worldwide

Siemens Global Weblogs

Language

 

Contact

MediaService Industries Blog

Entries » Blog » Combating noise - Acoustic chamber for optimizing noise in carsequipped with Simcenter software

Katharina Zoefeld |

Combating noise - Acoustic chamber for optimizing noise in carsequipped with Simcenter software

Linas-Montlhéry, France. Utac Ceram (UTAC) is located at Linas-Montlhéry, France, and offers services to all sectors involved in land-based movement. For example, Utac supports automotive manufacturers as they ensure noise levels from vehicles comply with regulations on noise pollution. To achieve this, Utac uses an acoustic chamber in which manufacturers can precisely measure and analyze the noise produced by their vehicles. The acoustic chamber is equipped with software from Siemens PLM Software.

 

Noise makes us sick - this is a scientifically proven fact. More and more governments are therefore tightening the regulations on maximum permissible noise levels. The limit for motor vehicles Europe-wide is currently 72 decibels (dB) and this is to be reduced to a maximum of 70 dB by 2020 and a maximum of 68 dB by 2024. The French company Utac Ceram (UTAC) supports automotive manufacturers in testing their vehicles for optimization opportunities and, ideally, in passing certification and homologation (approval) tests at the first time of asking. The company thus offers its customers, amongst other things, an ultra-modern acoustic chamber at its Linas-Montlhéry site in which noise generation and the causes of noise can be determined in the vehicle. Utac also supports manufacturers of hybrid and electric vehicle in the development of warning signals which indicate that the otherwise silent vehicle is approaching. The software utilized in the soundproof chamber comes from Siemens PLM Software.

 

Reproducible tests for accurate results

The unit is equipped with all-wheel drive rollers, a large number of microphones and the LMS Test.Lab and LMS SCADAS software solutions. The acoustic chamber is therefore able to simulate all types of vehicles passing by and to augment this in the test process, thus supplying highly accurate test results. The Indoor Pass-by Noise Tests allow the team to carry out repeatable tests in a controlled environment, irrespective of weather conditions. Vehicle speed and gear changes are automated which eliminates operator error. However, it is difficult to reproduce tire noise as this sounds different on a roller when compared to actual road conditions. This is where the Siemens solutions steps in. The LMS Test.Lab Pass-by Noise Testing software is part of the Simcenter portfolio and offers a tire noise calculation model which corrects tire noise data in accordance with procedures to ISO 362-3: 2016.

 

Acoustic warning signals

The acoustic chamber is not solely used for testing the reduction in pass-by noise. Utac supports manufacturers of hybrid and electric vehicles in equipping their vehicles with warning devices which produce a noise, also known as an Acoustic Vehicle Alerting System (AVAS). Utac uses LMS Test.Lab to define the minimum alarm level. According to Louis-Ferdinand Pardo, Acoustic Expert Leader and Department Manager, Electromagnetic Compatibility and Noise, Vibration and Harshness at Utac, there are many reasons to choose solutions from Siemens PLM Software. The software offers excellent data quality and processing capabilities for indoor pass-by noise tests. Using LMS testing solutions also ensures continuity and compatibility of tests performed indoors with tests executed outdoors. “We benefit from almost all the implemented functionalities of LMS Test.Lab, and despite being advanced users, we still appreciate the easy-to-use worksheets and intuitive workflow approach,” concludes Yori.

 

Captions:
Sensitive microphones, a set of all-wheel drive rollers and the LMS Test.Lab and LMS Scadas software solutions from Siemens PLM Software allow the team to simulate pass-by noises in the acoustic chamber.
Utac also runs tests in the acoustic chamber to support manufacturers of hybrid and electric vehicles as they fit their vehicles with noise-emitting warning devices.

 Please login to comment