Tools


Siemens Worldwide

Siemens Global Weblogs

Language

 

Contact

authors

    Postings written by : Eva Gansen

  • Eva Gansen | 10/09/2018

    Keine Chance für Cybercrime

    Schutz industrieller Steuerungen
    Cybercrime boomt. Laut einer aktuellen Studie des IT-Security-Anbieters McAfee kosten diese Angriffe Unternehmen jährlich rund 600 Milliarden Dollar – Tendenz steigend. Nutzen die verschiedenen Industrien die Digitalisierung bislang vor allem dafür, ihre Netzwerke und Steuerungssysteme zu vernetzen um Leistung, Zuverlässigkeit und Effizienz zu verbessern, gilt es nun, diese e...
  • Eva Gansen | 10/09/2018

    No chance for cybercrime

    Securing industrial control systems
    Cybercrime is booming. According to a current study by IT security vendor McAfee, these attacks cost companies some 600 billion dollars a year – and the trend is rising. Where various industries have hitherto used digitalization primarily to connect their networks and control systems together so as to enhance performance, reliability and efficiency, now it’s important to protect thos...
  • Eva Gansen | 17/05/2018

    Prozessindustrie 4.0: Neue Perspektiven gewinnen

    Keyvisual PCS7 V9.0
    Die Prozessindustrie blickt optimistisch in die Zukunft: Das Wirtschaftsministerium prognostiziert ein Wachstumspotenzial mit einem Volumen von ca. 30 Mrd. Euro bis 2020. Das Fraunhofer IAO geht von 30 Prozent zusätzlicher Wertschöpfung für die Chemieindustrie in den nächsten zehn Jahren aus. Was, wenn wir dieses Potenzial schon heute nutzen könnten?   So optimisti...
  • Eva Gansen | 17/05/2018

    Industrie 4.0 in the process industry: gaining new perspectives

    Keyvisual PCS7 V9.0
    The process industry is optimistic about the future: The Federal Ministry for Economic Affairs forecasts potential growth of around 30 billion Euros by 2020. Fraunhofer expects 30 percent additional added value for the chemical industry over the next ten years. What if we could use that potential today?     As optimistic as Fraunhofer is about the future, the research organization is...
  • Eva Gansen | 15/03/2018

    Turning measurement data into information

    When it comes to the future challenges of the global tank terminal industry, better information is one of the major issues. Improved, more timely and accurate information allows for precise process monitoring. It helps to prevent overspill and protects from media loss. It is also the enabling factor for better leak detection and a higher safety level.     For storage plant and termin...